Transformer Information

The most commonly used information about the transformer genie displays by default.

When the Advanced Properties box is checked, the table expands to include everything that is known about the selected transformer(s).

Basic transformer information includes:

Column

Description

State

Normal (), Warnings (), or Errors (). See the following table for explanations of errors.

Page

Name of the page on which the genie is found (displays only from the folder level).

ID

This is the breaker number, assigned when adding it to a page of a one-line.

Source Busbar

The number of the source busbar.

Dest. Busbar

The number of the destination busbar.

Sim. Source

This is the top source number used when adding the transformer.

Sim. Source 2

This is the bottom source number used when adding the transformer.

Transformer Errors

Before you use the drawing, correct all errors; otherwise the project might not compile and the animation will not work.

Errors that you might see for transformers are:

State

Solution

Errors ()

Source busbar number must be a number greater than 0.

The source busbar number is missing, or it is less than or equal to 0. Add or change the source busbar number.

Destination busbar number must be a number greater than 0.

The destination busbar number is missing, or it is less than or equal to 0. Add or change the source busbar number.

Source and Destination busbars must not be equal.

The source and destination busbars have the same number; change one number.

Either the Source or Destination Busbar number must exist (busbar may link to a Busbar, transformer, meter, source, or another breaker)

At least one busbar must be linked to this transformer.

If a top or bottom source is identified, it must be greater than 0.

The number for the top or bottom source for this transformer must be greater than zero (for voltage-level transformers) or must be left blank (for pass-through transformers).